博客

LX II Combination LCD Drawer and KVM-over-IP Switch

Posted on October 6, 2020 by Gento

Economical Remote Management and At-the-Rack Access in a Single Product!

Do you need web-based, remote management of computer and networking equipment?   Do you also need at-the-rack access of computer equipment?    And would you like an economical, easy-to-use product that can do both?

If so, Raritan’s Dominion LX II – LED combination LX II KVM Switch and T1700-LED LCD drawer models can do all of that and more!


Power Tip #5: Identify Failing Power Supplies

Posted on October 5, 2020 by Gento

Power supply failures are a leading cause of server failure. Additionally, most power supplies don't fail overnight but degrade over time. One key indicator of a degrading power supply is a declining power factor (PF). The PX3-5000 PDU series meters at each outlet. This metering monitors the power factor of each server. Most modern power supplies are rated for 85% (0.85 PF) or higher efficiency. Thus, setting a lower warning threshold for every outlet in use for a PF of 0.75 and a lower critical threshold for a PF of 0.65 can provide you with a preemptive alert to an impending power supply failure.

This alert can allow you valuable time to investigate and, if necessary, proactively turn the power supply off in a controlled scenario before an unexpected server outage occurs. This early alert can potentially help you to prevent a larger scale outage at the rack. Lastly, a degrading power supply over time consumes more power than average and can deprive power from other servers.


Power Tip #4: Create Additional Logins for All New Remote/Home Users

Posted on September 3, 2020 by Gento

With more staff working from home, it is the best protocol to provide them with their own user accounts instead of sharing the default admin account. Having individual user accounts makes all actions traceable.


Power Tip #3: How to Safely Trigger and Test the Alerting System

Posted on August 31, 2020 by Gento

While onsite staff might be unavailable to observe any on-premise issues, it is even more important to be assured that the alerting system you've set up works as intended. You can safely test the alerting setup without causing a real event.

We suggest you try this on just one PDU at first before all PDUs installed so you don't get flooded with alerts.

Setting up the test - lower the default thresholds for Inlet Voltage.


Blazing Virtual Media Speed for the Dominion KX IV - 101

Posted on August 24, 2020 by Gento

When we talk about the Dominion KX IV -101 as Raritan’s fastest KVM-over-IP switch, we are usually focused on its ability to support 4K video or 1080p video at 60 frames per second. But video isn’t the only area where the KX IV-101 shines!  Due to its all-digital architecture and its direct USB connection to the target computer, the KX IV-101 supports virtual media much faster than our current generation Dominion KX III switches.  


Page 3 of 58 pages  < 1 2 3 4 5 >  Last ›

力登官方微信公众号

力登官方微信公众号
cn-blogfollow

近期活动

Data Cloud India
February 5-6, 2020  •  Mumbai, India
Industrial Automation
April 24, 2020  •  Tainan, Taiwan
DigiTimes Data Center Forum Taipei
May 8, 2020  •  Taipei, Taiwan
Cloud & Data Center Convention (Wmedia)
May 14, 2020  •  Manila, Philippines
Industrial Automation
May 14, 2020  •  Taipei, Taiwan

View all Events

力登最新新闻

力登公司推出MasterConsole®数字双显示器KVM切换器
Posted on February 18, 2021
Legrand Data, Power and Control Division Announced as Finalist in Six Categories at DCS Awards 2020
Posted on November 9, 2020
力登公司(Raritan)推出新型智慧型机架控制器(SRC),用于智能地管理数据中心和关键基础设施中的环境和安全信息
Posted on November 9, 2020
Legrand India Launches Datacenter Infrastructure Solution for the addressable market size of INR 3000 crores
Posted on August 23, 2020
力登公司推出面向中小型企业的全新一代KVM-Over-IP交换机和串行访问
Posted on March 16, 2020

View all news