The Raritan Blog

Mobile App For Your KX IV-101

Jessica Ciesla
October 15, 2019

Raritan’s new KVM app was developed to help customers easily install and configure the Dominion KX IV – 101.  Thanks to the newly released KVM Mobile App, installations and configurations are now even easier to complete. This innovative tool not only increases efficiencies, but also helps customers more effectively control, secure, and manage multiple locations.

“Raritan KVM” Mobile App for Local Installation and Configuration

The core component of Raritan products is to create environments that are not only secure but are also scalable. For example, the Dominion KVM-over-IP switches are designed to provide both on-site rack access, as well as remote control and effective management via LAN, WAN, and the Internet. The latter capabilities have now been enhanced thanks to the newly released mobile app.

The Raritan KVM Mobile App is just the latest innovation to help customers gain the actionable insights that they need for smarter decision-making. It is now available on the iPhone and iPad and can be downloaded from the Apple App Store onto your Apple device. Like the Raritan PDView App that is used to easily configure Raritan's best-in-class intelligent PDUs, so too is the latest app built to help install and configure Raritan's Dominion KX IV -101 products.

Download the App

To download the app, simply search for "Raritan KVM" within the Apple App store. To begin using the app for streamlined installation and configuration, complete the following steps.

•    Launch the app on your iPhone or iPad device.
•    Connect your iPhone or iPad to the USB-A port on the Raritan KVM switch.
•    You will see a login screen on the KX4-101.
•    Login to the KX4-101 using your designated username and password.
•    Upon successfully logging in you will see a Java-free User Interface.
•    Use the Java-free User Interface to configure the KX4-101.

It is important to note that thanks to the Raritan KVM Mobile App the above six steps, as well as the initial configuration of the KX4-101 can be completed easily and quickly. Additionally, all of the administrative settings on the KX4-101 can be changed. You can also use the mobile app to easily make changes in the future.

To learn more about the benefits of the Raritan KVM Mobile App, contact a member of the Raritan team today.
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
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications
Posted on March 5, 2024