About Us

Raritan Reveals The MasterConsole® Digital KVM Switch DUAL

Posted on February 26, 2021

New Switch Allows Users to Productively Work With Dual Displays With Borderless Mouse Switching

Schiedam (The Netherlands) – February 23, 2021 –  Raritan®, a brand of Legrand® and a leading provider of intelligent data center management and rack power distribution solutions, today announced the MasterConsole Digital-DUAL KVM switch (MCD-DUAL). The company’s dual monitor KVM switch consolidates access and control of multiple dual-head servers with a single console supporting dual-display output, HDMI, DisplayPort, DVI, and VGA video. These features make the switch ideal for art and graphic design, broadcast and customer service needs, control rooms, engineering, finance, manufacturing, and other multi-screen requirements.

The MCD-Dual comes in two, one-user models, the MCD-104 DUAL which connects to 4 dual-headed servers, and the MCD-108 DUAL which connects to 8 dual-headed servers. Both can be cascaded into two levels to support up to 64 connections. The dual-monitor KVM provides a friendly on-screen display and hotkeys to access connected computers. In addition, the convenient, borderless mouse switching allows users to move the mouse to strike the monitor’s edge, and then the mouse will automatically move to the next port. Other features include:

● Simple, plug-and-play installation and configuration.
● AutoScan allows users to scan servers at variable rates and also enables AutoSkip to bypass inactive channels.
● “Keep-alive” technology allows users to add, remove and hot-swap components without interruption to the live servers.

“Raritan’s MasterConsole Digital-DUAL KVM switch is a continuation of our successful line of MasterConsole devices that provide a centralized point-of-access to multiple servers without the expense and clutter of a dedicated keyboard, mouse, and monitor for each computer or server,” said Richard Dominach, Director of Product Management, Raritan. “With this new version, the MasterConsole now supports dual-headed servers with two video outputs. The MCD Dual models are truly unique in their support for dual-head servers using HDMI, DisplayPort, DVI and VGA video formats—all in a single switch!”

Visit www.raritan.com/eu or email sales.europe@raritan.com for more information.

View by Category
Monthly Archives
More Recent News
‘At-the-Rack’ KVM-over-IP Access in Branch Locations
Posted on September 15, 2020
New KVM-Over-IP Switch with Serial Access for SMBs
Posted on March 30, 2020
Raritan ranked as the global leader in KVM-over-IP Switches
Posted on November 25, 2019
Extended IT rack power mapping with Raritan locking solution
Posted on October 24, 2019
KVM-over-IP Switch with Enhanced Performance and 4K HD
Posted on May 21, 2019