About Us

Raritan Introduces High Performance, IP User Station for Broadcast and Control Room Operations

Posted on November 30, 2015

—Industry’s most productive and powerful user interface to view, access, and control workstations and servers remotely—

SOMERSET, N.J. — (November 30, 2015) — Raritan—a leading provider of intelligent data center management, KVM and rack power distribution solutions—today introduced a new IP User Station for the Dominion® KX III digital KVM switch.  Together they provide technicians, operators, engineers and IT professionals with an economical IP-based solution for high-performance remote access to IT devices with the industry’s most productive and powerful user interface. 

Ideal for the work done in broadcast studios, control rooms, and labs, as well as offices and data centers, the KX III User Station solution, supports two 1920 x1080 video sessions at 30 frames per second, sub-second switching between servers, and eight or more simultaneous KVM-over-IP sessions over single or dual monitors.  Unlike other high-performance KVM solutions that require a separate network, users can access and control multiple servers and other equipment over the corporate LAN and/or WAN.  Moreover, the KX III’s web browser interface enables authorized users to access connected equipment using their laptop or PC while traveling or for emergency access from home.

“The new IP User Station offers versatility; it can be used to replace or supplement expensive, inflexible broadcast systems or be used as a console in a lab, studio or operations center.  It can support the high-performance needs of technicians or operators, as well as BIOS-level access and virtual media for IT and broadcast engineers,” said Richard Dominach, Director of Product Management at Raritan.  “Like the KX III the new user station was designed to boost productivity by delivering the best performance, reliability, usability, compatibility, and security.  Analog (VGA) and digital video formats, including DVI, HDMI and DisplayPort, are all supported.”

The KX III User Station appliance can be conveniently located – in the same room or miles away from the KX III switches connected to servers and other equipment.  Using economical and scalable Cat5, Ethernet, and TCP/IP technologies, any User Station can access any KX III switch throughout the enterprise.  The User Station can sit on a desk, be mounted onto a standard 19” rack, or VESA-mounted on the back of a monitor.

About Dominion KX III
Raritan’s Dominion KX III enterprise-class, secure KVM-over-IP switches provide BIOS-level remote management of up to 64 multi-platform servers and serial-based devices in a single switch.  With BIOS-level access, a server is always accessible and can be remotely rebooted in the event a server’s operating system is not working.

Availability and Pricing
Available worldwide through Raritan’s channel partners, the U.S. list price for the KX III User Station is $999.  Together with the Dominion KX III digital KVM switches, the Raritan solution is a fraction of the price of many broadcast systems. 

For more information visit: www.raritan.com/UserStation

About Raritan
Raritan, a Legrand Company, is a proven innovator of power management and KVM-over-IP solutions for data centers of all sizes.  In over 76 countries and 50,000 locations worldwide, Raritan’s award-winning hardware solutions increase energy efficiency, improve reliability, and raise productivity.  For more information, visit us at Raritan.com or follow us on the Raritan blog.
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
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications

—ISO27001 certification delivers assurance to the security of thoroughly tested data, power and control devices from Legrand brands, including the Raritan®, Server Technology® and Starline® brands.

Posted on March 5, 2024
Legrand Releases Version 4.0 of Raritan’s Industry-Leading Secure KVM Switches, Raising Bar for Secure Desktop Access

—Raritan Secure Switches (RSS) meet the stringent requirements of NIAP 4.0 Peripheral Sharing Device and can be implemented to protect government and private sector data.

Posted on July 31, 2023
Legrand Revitalizes Data Center Sector with Two Revolutionary Intelligent Rack PDUs

— Offered by Legrand brands Server Technology and Raritan as the PRO4X and PX4, the new intelligent PDUs offer unparalleled visibility, flexibility, density and security for ever-changing rack power and infrastructure requirements —

Posted on May 1, 2023
Raritan Reveals The MasterConsole® Digital Dual KVM Switch

— New Switch Allows Users to Productively Work With Dual Displays With Borderless Mouse Switching —

Posted on February 18, 2021