{announcement-message}

Resources

Application Briefs

Learn how Raritan products and solutions can serve the real-world needs of your business.
Filter by:
KVM Solution for Semiconductor Manufacturing

Modern semiconductor fabs have hundreds or thousands of complex machines that must be efficiently utilized, monitored, maintained and repaired. In this application brief, we discuss how KVM-over-IP switches help maintain these complex machines to provide increased productivity, quality, and efficiency in a clean room environment.

Branch Circuit Monitoring: Power Monitoring and Measurement in Production Facilities

This application brief will address many of the power infrastructure challenges that are common in factories, production facilities, and large distribution centers. Provided will be real life, on-site experiences as well as an outline of steps required to overcome these costly challenges. In many cases, the implementation of affordable and easy-to-install modular technology has helped address these issues.

Reduce CAPEX and Prevent Downtime by Hardwiring Your Rack PDUs

Want to dramatically reduce your CAPEX spend on your next data center buildout? Consider deploying hardwired rack power distribution units (rack PDUs).

Use Raritan’s Intelligent Rack PDUs to Efficiently Power Cisco’s Nexus 7718

Use Raritan’s PX iPDU Series to reliably distribute power for up to sixteen power supplies. The Cisco Nexus 7718 is an 18-slot chassis with 18 front-accessible vertical module slots and front-to-back airflow and an integrated cable management system.

Use Raritan’s Intelligent Rack PDUs to Efficiently Power Cisco’s Nexus 7710

Use Raritan’s PX iPDU Series to reliably distribute power for up to eight power supplies. The Cisco Nexus 7710 is a 10-slot chassis with 10 front-accessible horizontal module slots and front-to-back airflow and an integrated cable management system.

Use Raritan’s Intelligent Rack PDUs to Efficiently Power Cisco’s Nexus 7018

Use Raritan’s PX iPDU Series to reliably distribute power for up to four power supplies. The Cisco Nexus 7018 is an 18-slot chassis with 18 front-accessible horizontal module slots and side-to-side airflow and an integrated cable management system.

Use Raritan’s Intelligent Rack PDUs to Efficiently Power Cisco’s Nexus 7010

Use Raritan’s PX iPDU Series to reliably distribute power for up to three power supplies. The Cisco Nexus 7010 is a 10-slot chassis with 10 front-accessible vertical module slots and front-to-back airflow and an integrated cable management system.

Addressing Retail Server Downtime
If a server fails at a remote retail store location, it almost always causes unacceptable downtime, and demands additional manpower, travel time and travel expenses. Now Raritan can help, with a proven, secure, out-of-band solution that can resolve problems remotely.
Dealing with Field Technician Overload
Few people work as hard as IT field technicians. Faced with challenging environments and limited resources, they’re constantly under pressure to solve problems quickly and efficiently. Now they can. Armed with a laptop and the Dominion® KX II-101, they can connect to any target server without the need for a crash cart.
Cloud Infrastructure (Remote) Management Solution
While virtualization offers flexibility and cost reduction, IT administrators considering a cloud-based architecture still need to control, manage and secure IT infrastructure. Before adopting the cloud, consider Raritan’s Cloud Infrastructure (Remote) Management Solution – it centralizes management and provides out-of-band remote access of critical IT resources from anywhere.
Remote Management and Control for Business Continuity
Data centers are susceptible to a wide variety of disasters, attributable to human error, system breakdowns and other factors. In these instances, secure remote access and control are essential to minimizing fallout. Raritan’s Business Continuity and Disaster Recovery Solutions offer IT managers the tools to quickly access and recover virtually any server.
Broadcast
The demands of broadcast programming require 24/7 access to playlists and content, without exception. When on-site IT staff is not a possibility and physical space is limited, remote access management provides an ideal solution. To centralize management and gain out-of-band remote access to critical IT resources, look no further than Raritan’s Remote Broadcast Server Management and Control Solution.
Labs
In order to accommodate weekend shutdowns while maintaining efficiency and minimizing costs, lab managers are increasingly relying on remote management options. To do so, they require tools that offer reliability and security, while enabling automation, scheduling and power management – Raritan’s Lab Server Management Solution provides exactly that.
Kiosk Remote Server Management
Businesses that use kiosks such as ATMs to serve their customers have many unique support and maintenance challenges. To ensure that ATMs are secure and available 24/7 – security, energy, environmental and visual controls are all necessary. Learn how Raritan’s solution can help.
Remote Management and Control for Disaster Recovery and Business Continuity
While IT managers can’t predict when disaster will strike, they can take steps to ensure that service will be restored as quickly as possible when it does. Raritan’s Business Continuity and Disaster Recovery Solutions helps IT staff to quickly, efficiently and accurately troubleshoot, diagnose and repair post-disaster system failures.
dcTrack Full Power Chain and Network Connection Management
Despite the overall increase in data center capability, managers are often asked to improve uptime and capacity utilization. In order to safely meet these demands, full power chain and network connection management must be leveraged.
Avocent DSR Integration for a Smooth Migration to Raritan
With Raritan’s Dominion KX II and CommandCenter Secure Gateway (CC-SG) integration capabilities, Data Center Administrators and Lab Mangers can access the servers and PCs controlled by both Avocent DSR and Raritan’s Dominion KX II switches from a single Raritan solution.
Data Center Moves
With the many changes that will take place during a data center move including updating inventory records and defining new space and power requirements, a tool that will help guide your new site’s growth, provide information to enable informed decisions on capacity and asset placement, and help keep your new data center healthy from day one is a must. Learn how DCIM can help in your new data center.
Remote Access and Control SIPRNet Solution
To ensure the secure transmission of classified and secret information, the U.S. Government has mandated that beginning in April, 2013 all access to military, intelligence, and other agency classified systems will require the use of a limited-access computer network Secret Internet Protocol Router Network (SIPRNet) token. Learn how KVM solutions provide secure, high-speed remote access and control of multiple classified systems and meet the mandate.
Management and Wireless in the Data Center
Raritan and Wi-Fi access point vendor Xirrus have created a white paper which presents a sophisticated wireless monitoring and management solution for data centers. There are numerous advantages to using Wi-Fi for data center infrastructure management (DCIM) instead of hardwired Ethernet connections. Ethernet requires additional cabling, switches, rack space and more. In fact in many cases a complete Wi-Fi solution costs less than just the cost of pulling cables for Ethernet.
Development and Test Labs
Efficient computer-based development and test labs are essential to companies who must continuously introduce innovative new products into the marketplace. To succeed, labs managers must overcome severe challenges to access and configure lab equipment and automate systems while continuing to decrease energy costs. Learn how Raritan helps the world’s most innovative companies increase their productivity resulting in faster time-to-market.