About Us

Raritan Introduces Economical Intelligent Rack PDU with True kWh Energy Metering

Posted on September 20, 2010

—New PX-1000 Series delivers cost-effective energy intelligence to data centers—

SOMERSET, N.J. (September 20, 2010) – Raritan today added a new family of intelligent rack power distribution units (PDU), the Raritan PX-1000 Series, to its power management portfolio.  Setting a new performance standard, the high-quality, metered-PDU PX-1000 comes with built-in intelligence, integrated support for optional environment sensors, Web-based energy performance tracking capabilities and a multitude of security features. 

“The PX-1000 is a smart choice for companies that want accurate and continuous power monitoring in order to get to the heart of power issues—such as identify ways to reduce energy costs, orchestrate efficient cooling among racks, and optimize capacity,” said Herman Chan, Director of Raritan’s Energy Management Business.  “Raritan continues to apply its unmatched combination of engineering capabilities, technology innovation and global partner ecosystem to deliver solutions that help companies manage their data center power and cooling resources more efficiently.” 

The PX-1000, and Raritan’s other intelligent rack PDUs, gather extensive and accurate power information, including data on voltage, current (Amps), power factor, apparent power (kVA), active power (kW), environmental temperature and humidity and energy consumption in kilowatt hours (kWh).  To make it easy for data center operators to view power activity, real-time information can be seen on the PDU’s LED display at the rack and from a remote user interface via a Web browser.  User-configurable critical and non-critical power and environmental thresholds can be set, and alerts sent so data center managers can take corrective action.

PX delivers the industry’s most accurate measurement—with ISO/IEC +/- 1% billing-grade accuracy—on the important kWh metric; whereas other solutions only measure current (Amps) or determine kWh through calculations and assumptions, instead of real-time measurement.  “kWh is key to knowing the real cost of power usage and carbon footprint,” said Chan.  “With the introduction of our new PX-1000 Series, Raritan is now offering true energy metering technologies for data centers of all sizes.”

Also new with the PX-1000 is the industry’s first auto-flip PDU display that changes the orientation of the LED display when the PDU is rotated, which provides added rack installation flexibility .  In addition to Ethernet, the PX-1000 comes with additional ports—including USB-A (host), USB-B (device), Feature/KVM, and DB9 RS232 serial. 

All PX models are fully supported by Raritan’s Power IQ® Energy Management software that provides additional monitoring and management capabilities.  Also available are optional environmental sensors that are automatically detected and displayed as soon as they are plugged into the PX-1000.  Raritan’s sensors track temperature and humidity at the rack to help eliminate over cooling and hot spots. 

As part of the PX-1000 introduction, Raritan unveiled a free sensor promotion.  With each PX-1000 purchased this year, customers will be given a free temperature sensor. 

PX-1000 is available worldwide starting today from Raritan’s channel partners.  List price starts at $449.  More information on Raritan’s power solutions can be found at www.raritan.com/energy-metering/

About Raritan’s Intelligent Rack PDUs
Raritan’s intelligent rack PDU portfolio is the largest in the industry and includes single-phase, three-phase, high power (400V), outlet-metered, outlet-metered and outlet-switched, and metered rack PDUs and inline power meters to meet the needs of diverse IT environments. 

Raritan PX intelligent rack PDUs are fully compatible with Raritan’s Power IQ energy management software for analyzing power usage and tracking trends.  Enterprise-wide data gathered by Raritan’s intelligent PDUs, third-party rack PDUs, and in-line meters enables Power IQ’s analytics to calculate and chart active power, energy consumption, cost and carbon footprint for servers and other IT devices.  Power information is presented in user-configurable graphs and reports that can be accessed from anywhere with Power IQ’s Web-based dashboard.  Graphs can easily depict which devices are consuming the most energy, whether power conservation efforts are working, and if there are hot spots or over-cooled areas.  Power IQ is offered as a virtual and a hardware appliance.  A free trial version of Raritan’s Power IQ software is available at http://www.raritan.com/power-iq-download/

About Raritan

Raritan is a proven innovator of power management, infrastructure management, KVM and serial solutions for data centers of all sizes.  In more than 50,000 locations worldwide, Raritan’s award-winning hardware and software solutions—including intelligent PDUs, energy management software, KVM-over-IP and Serial-over-IP access products—provide IT and facility directors, managers and administrators with the control they need to increase power management efficiency, improve data center productivity and enhance branch office operations.  Based in Somerset, N.J., Raritan has offices worldwide serving 76 countries.  For more information, visit Raritan.com.  Raritan is an active member of the Green Grid, Climate Savers Computing Initiative, and the Leadership in Energy and Environmental Design (LEED) associations. 

Raritan’s power management solutions won five key industry awards in 2010 and
were recognized by the EPA for contributions to the agency’s data center initiative.
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
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications

—ISO27001 certification delivers assurance to the security of thoroughly tested data, power and control devices from Legrand brands, including the Raritan®, Server Technology® and Starline® brands.

Posted on March 5, 2024
Legrand Releases Version 4.0 of Raritan’s Industry-Leading Secure KVM Switches, Raising Bar for Secure Desktop Access

—Raritan Secure Switches (RSS) meet the stringent requirements of NIAP 4.0 Peripheral Sharing Device and can be implemented to protect government and private sector data.

Posted on July 31, 2023
Legrand Revitalizes Data Center Sector with Two Revolutionary Intelligent Rack PDUs

— Offered by Legrand brands Server Technology and Raritan as the PRO4X and PX4, the new intelligent PDUs offer unparalleled visibility, flexibility, density and security for ever-changing rack power and infrastructure requirements —

Posted on May 1, 2023
Raritan Reveals The MasterConsole® Digital Dual KVM Switch

— New Switch Allows Users to Productively Work With Dual Displays With Borderless Mouse Switching —

Posted on February 18, 2021