About Us

Raritan Introduces Secure Access Solution with Integrated SIPRNet Smart Card Reader

Posted on February 11, 2013

SOMERSET, N.J.  (February 11, 2013) — Raritan today introduced the industry’s first remote access-and-control KVM switch with an integrated SIPRNet token reader.  The U.S. Government has mandated that SIPRNet hardware tokens be used to access systems on the Secret Internet Protocol Router Network by April 2013.

Similar in appearance to a smart card or CAC (common access card), a SIPRNet token is cryptographically bound to the user’s identity and contains individual PKI (public key infrastructure) certificates used for network logon, Web site authentication and secure e-mail.  Credentials stored on hardware tokens are only accessible using specialized software and card readers.

Raritan’s new Paragon KVM solution for government customers has three key components:  a Paragon II Enhanced User Station with an integrated SIPRNet Card Reader, an updated Paragon II USB Computer Interface Module, and the enterprise-class Paragon II Cat5 KVM switch, which is a proven KVM workhorse used widely by government and military agencies to access servers.

Data center servers and other IT equipment equipped with the required middleware software can be centrally accessed using the new Paragon SIPRNet card-reader solution.  Once a government IT professional is authenticated they can access and control servers and other networked devices using secure, high-speed, BIOS-level access.  Paragon also provides a consolidated view of all Paragon-connected servers and devices.

“We have built upon the extensive expertise that Raritan had developed in delivering the industry’s first and most widely deployed CAC KVM solution,” said Richard Dominach, Senior Product Manager for Raritan.  “Recognized for the security and reliability of our products, we are one of the first to deliver a secure KVM solution for accessing systems on SIPRNet.” 

Raritan’s new solution has been tested extensively by multiple customers, who have verified that the SIPRNet system meets their needs for access to classified systems.

For additional security measures, Paragon II does not store or cache smart card data, requires re-authentication when switching between servers, and allows access to a given server by only one user at a time.  The Paragon II solution is on the United States GSA schedule of approved FIPS 201 products.  More on the solution can be found at www.raritan.com/SIPRNet

About Raritan (Raritan.com)
Raritan is a proven innovator of energy and infrastructure management solutions for data centers of all sizes.  In more than 50,000 locations worldwide, Raritan’s award-winning hardware and software solutions—including intelligent rack PDUs; DCIM software; energy management software; KVM-over-IP and Serial-over-IP access and control products—provide IT and facility directors, managers and administrators with the control they need to increase power management efficiency, improve data center productivity and enhance branch office operations.  Based in Somerset, N.J., Raritan has offices worldwide serving customers in 76 countries.  Visit us at Raritan.com or follow us on the Raritan blog. 
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
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications

—ISO27001 certification delivers assurance to the security of thoroughly tested data, power and control devices from Legrand brands, including the Raritan®, Server Technology® and Starline® brands.

Posted on March 5, 2024
Legrand Releases Version 4.0 of Raritan’s Industry-Leading Secure KVM Switches, Raising Bar for Secure Desktop Access

—Raritan Secure Switches (RSS) meet the stringent requirements of NIAP 4.0 Peripheral Sharing Device and can be implemented to protect government and private sector data.

Posted on July 31, 2023
Legrand Revitalizes Data Center Sector with Two Revolutionary Intelligent Rack PDUs

— Offered by Legrand brands Server Technology and Raritan as the PRO4X and PX4, the new intelligent PDUs offer unparalleled visibility, flexibility, density and security for ever-changing rack power and infrastructure requirements —

Posted on May 1, 2023
Raritan Reveals The MasterConsole® Digital Dual KVM Switch

— New Switch Allows Users to Productively Work With Dual Displays With Borderless Mouse Switching —

Posted on February 18, 2021