About Us

Raritan Unveils KVM-over-IP Switch with Enhanced Performance and 4K Ultra HD

Posted on April 4, 2019

LAS VEGAS, NV (April 8, 2019)Raritan® — a brand of Legrand, and a leading provider of intelligent data center management and rack power distribution solutions — today announced a more powerful and flexible KVM-over-IP switch and User Station to support the demanding needs of today’s broadcast studios, control rooms, labs, data centers — and in just about any place that secure and reliable access to equipment is needed.

With 4K Ultra HD (UHD) video resolutions and super-fast response times, Raritan’s new Dominion KX IV-101 digital switch is more powerful and flexible than any other KVM‐over‐IP switch. The Dominion KX IV provides unblocked high-performance access to servers and workstations; and, up to three times faster virtual media transfers for remote software installations and other tasks. Users can access and control equipment via a User Station, PC, or laptop. 

Performance also was boosted in Raritan’s new KX IV User Station recommended for customers using 4K resolution and requiring multiple KVM sessions. It supports three connected monitors and provides three times more processing power than previous models. 

“With our fourth- generation Dominion KX, we’ve created an all-new KVM-over-IP architecture to support the most demanding and challenging environments and applications,” said Richard Dominach, Director of Product Management at Raritan. “The KX IV-101 meets the high-performance needs for broadcast, control rooms, and other dynamic applications, and provides flexible IP-based remote access required for remote offices, facilities, colo’s and manufacturing. Our engineers have created the most advanced KVM platform ever, leveraging our 30 years of KVM development and the innovative technologies from Raritan’s Xerus™ Technology Platform.”

Unveiling at NAB Show
The new Dominion KX IV-101, a KVM-over-IP switch which connects to a single computer, providing “un-blocked” access and control to multiple users, will be debuting at this week’s NAB Show for media, entertainment, and technology professionals.  Also, on display is Raritan’s Dominion KX III multi-port KVM switches and the new Dominion KX IV User Station. 

About the Dominion KX IV
The KX IV is a flexible, IP-based solution for operations, broadcast engineering, and IT users.  Unlike other high-performance KVM solutions that require a separate network, Dominion KX users can access and control equipment using a LAN, WAN, and, even, the Internet for emergency IT access. 

With the Dominion KX’s BIOS-level access, a server is always accessible and can be rebooted remotely in the event a server’s operating system is not working. 

The Dominion KX IV enhancements include:

  • Up to 4K video resolutions: 1080p, 1440p, 1600p.
  • Faster frame rates — up to 60 frames per second.
  • High-quality 4:4:4 color.
  • Digital audio via HDMI.
  • Faster virtual media transfers.
  • New KVM app to configure the KVM IV using Apple mobile devices.

The all-digital Dominion KX IV also has many of the popular Dominion family features, such as absolute mouse synchronization, LDAP/Radius/AD authentication, AES encryption, eight simultaneous KVM-over-IP sessions, and Java-free access on laptops and PCs.

Visit here for more information about the KX IV-101.

About Raritan
Raritan, a brand of Legrand, is a global leader in intelligent rack PDUs, KVM switches, and other data center infrastructure monitoring and management solutions. Raritan’s innovations improve the reliability, efficiency, and intelligence of data centers and server rooms around the globe — including those of the top Fortune 500 companies, such as Cisco, Dell, Google, HP, IBM, Intel, and Microsoft. To learn more, visit Raritan.com, LinkedIn or Twitter.

About Legrand and Legrand, North and Central America
Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines that includes AFCO Systems, C2G, Cablofil, Chief, Da-Lite, Electrorack, Finelite, Luxul, Middle Atlantic Products, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Sanus, Solarfective, Vaddio, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819) www.legrand.us.

# # #

All product and company names herein may be trademarks of their registered owners.

View by Category
Monthly Archives
More Recent News
Legrand Wins Back-to-Back Awards for Intelligent Rack Power Distribution Innovation
Posted on June 25, 2024
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications

—ISO27001 certification delivers assurance to the security of thoroughly tested data, power and control devices from Legrand brands, including the Raritan®, Server Technology® and Starline® brands.

Posted on March 5, 2024
Legrand Releases Version 4.0 of Raritan’s Industry-Leading Secure KVM Switches, Raising Bar for Secure Desktop Access

—Raritan Secure Switches (RSS) meet the stringent requirements of NIAP 4.0 Peripheral Sharing Device and can be implemented to protect government and private sector data.

Posted on July 31, 2023
Legrand Revitalizes Data Center Sector with Two Revolutionary Intelligent Rack PDUs

— Offered by Legrand brands Server Technology and Raritan as the PRO4X and PX4, the new intelligent PDUs offer unparalleled visibility, flexibility, density and security for ever-changing rack power and infrastructure requirements —

Posted on May 1, 2023
Raritan Reveals The MasterConsole® Digital Dual KVM Switch

— New Switch Allows Users to Productively Work With Dual Displays With Borderless Mouse Switching —

Posted on February 18, 2021