主页 » 博客
Posted on April 10, 2013 by Gento
High-power requirements for data centers include racks filled with 1U “pizza box” servers or multiple blade server chassis in one rack. Network storage devices can also drive high demand for power.
Many data center managers are doing a good job conserving energy but, average power consumption at the rack may still go up. In fact, the increased efficiency means more power is available to support data center growth. This webinar will examine how to determine and design for peak actual power demand and the most efficient and reliable approaches for delivering power, especially when deploying blade servers.
Date: Thursday, April 25, 2013
Time: 11:00 AM ET
Register: https://www1.gotomeeting.com/register/829819449
Posted on April 9, 2013 by Gento
Despite the growing ubiquity of 3-phase power distribution (at 208V) in North American data centers, data center operators are still not sufficiently fluent with the real-world capacity implications of 3-phase power in their cabinets.
The principal reason is because—at 208V—the math required to understand 3-phase power distribution at the cabinet is completely counter-intuitive.
THE TWO MOST COMMON QUESTIONS I GET are some form of the following:
Whatever you think is reasonable in your head is, in fact, not actually the way it works. So the answer to both of the above questions is, “no”.
In a previous post, I attempted to explain at a lower-level the reasons why this is true—including a link to a very useful Excel spreadsheet to help you calculate 3-phase rack PDU loading and capacity planning..
But I realize that most people are like me (lazy). You don’t need to know the electrical rationale for the counter-intuitive math, you just need to know the answers! So in this post you will find just the main information you need to do simple capacity planning (without explaining the reasons why). I guess I really should have posted this first. Whoops!
THE SHORT VERSION: 2 Primary Tips
1. If you don’t totally, 100% understand 3-phase power distribution, it is best if you do NOT think or speak in terms of amps. In all likelihood, you will say something incorrect that confuses your electrician.
Instead, think about how many watts your equipment consumes, and how many watts your 3-phase power strip can provide. Watts are universally comparable, regardless of the supplied electrical configuration available at your rack: both your power strip manufacturer and your IT equipment vendor will tell you how many watts can be supplied. No matter what voltage you use; the rated current (amps); or whether you have 1-phase power or 3-phase power; etc… you can always compare watts.
If you absolutely must think using amps (i.e., “My Dell salesperson says this server will draw a maximum of 1.4A; and that’s all he will tell me.”), then I strongly suggest you: (a) download and use our 3-phase calculator here; and (b) consult the right-most column of the following cheat-sheet.
2. Print out this chart, pin it on your bulletin board ... and trust no other document on earth. (Click to view as high-resolution PDF).
SOME OBSERVATIONS
THIS INFORMATION IS VENDOR NON-SPECIFIC
Please note that all the information in this post is not specific to Raritan power strips—but is vendor-agnostic… it’s just math. (Of course, if you do find this information beneficial, I sure would appreciate your considering Raritan as a potential provider for critical power distribution in your next build.)
Learn the most innovative features of rack power distribution units.
Posted on April 3, 2013 by Gento
Raritan’s iPDUs plus Power IQ® Software lead to lower Data Center Opex
What if, the next time you opened your home electric bill, instead of a lump sum of kilowatt-hours, you found an itemized list of every electrical appliance — down to each and every light bulb—that drew power that month, and how much you’re spending to run it? Instead of shrugging and hunting down your checkbook, you would have useful information you could use to drive that bill down.
You would know what it’s costing to keep that spare freezer in the basement. You’d know exactly who left the garage light on all night, or if your air conditioner was really living up to its energy star rating. You could take steps to avoid overpaying, enforce family policies, and make smarter purchases.
That’s just a glimpse of what can be done now for the data center, with the wealth of information pumped out by Raritan iPDUs. These units continually generate tons of real-time data down to the circuit-breaker or the outlet level, if you need it. In addition to your industry-standard amperage reading, these intelligent strips can push a tremendous amount of granular data through one IP drop. Connected to environmental sensors, they can continually report on temperature, humidity, open-closed contact status, airflow, and CO2 level as well. They can even stream a web cam feed.
Far from being TMI, this data is what empowers you equip every rack with just the right amount of cooling, for example. And that’s not small potatoes: According to Gartner, data centers save four percent of their cooling budget for every degree they can raise ambient temperature. A related example: that iPDU can also tell you —with 1% accuracy— how many kwH you’re consuming every month to power any particular blade server. And since you’re billed in KwH, you’ve now got an apples-to-apples comparison between consumption and cost, or between different hardware models and configurations.
Knowing which aisles are hot, and which are not
With a clickable, real-time display on the PDU and the capacity for up to eight temperature and eight humidity sensors, you can discover aisle-specific hot spots to more accurately concentrate your cooling. You can determine if there’s a systemic problem, or just a vent, for example, that’s been blocked by a carelessly placed briefcase. You can keep humidity levels high enough to prevent electrostatic discharge, and low enough to discourage hardware corrosion and with that, early system and component failure.
Raritan’s Power IQ software is what takes in all this data from Raritan’s, as well as competitors’, intelligent PDUs, analyzes it, and makes it actionable. It can aggregate and analyze data across multiple centers in multiple sites, and even generate ODBC-exportable reports.
In my next blog, we’ll talk a bit more about Power IQ and Raritan’s EMX controller, which allow you to set thresholds, alerts, and generally inject invaluable smarts into one of the dumbest things in your data center—the rack.
Click here to learn more about Raritan’s data center power management solutions
Click here to follow our group on Linkedin
Posted on April 1, 2013 by Gento
Hear 40+ Speakers, Including New Industry Voices & Active Data Center Real Estate & Technology Firms
With the combined economic recovery and rapid rise in interest in the data center real estate and technology infrastructure sectors, there could not be a more important forum to separate fact from fiction.
Date: Thursday, April 11, 2013
Location: Santa Clara Convention Center, 5001 Great America Parkway, Santa Clara, CA 95054
Stop by the Raritan table to see the latest power management solutions. You’ll be entered into a drawing for a blu-ray player. For more details and to register, please visit http://cre-events.com/dcnorcal2013/.
Posted on March 27, 2013 by Gento
In a recent study by Carnegie Mellon University it is believed that video game consoles cost U.S. homeowners more than $1.24 billion per year. A significant portion of that cost is due to 10.8 terawatt-hours of power consumption (is that right?), according to their study.
We can all agree wasted energy adds up quickly when you have gamers starting at a very young age and continuing into adulthood. No worries, just like anything else there is a solution and believe it or not it is SIMPLE. All you games really need to do is fully turn off the console when you are done. And don’t worry, your game will save. It’s no longer the days of the Atari 2600 when all your settings and achievements get lost when you power down.
Sony and Microsoft have worked to make their products more energy efficient however;, both the Xbox 360 and PS3 still draw significant power. If gamers choose to let their consoles go into standby mode and not completely power them down as they often do, the game console can continue to consume about 75 watts of power..
To provide the consumer with a better understanding of this high cost and wasted power issue, game console manufactures can create efficiency charts that show the power wasted over a certain period of time if the console does not get completely powered off.
Manufacturers can utilize Raritan iPDUs to implement power efficiency testing methods that can build a framework for game console power utilization efficiency standards.