力登公司的制造业解决方案可以为成百上千台半导体制造设备提供安全、可控的本地以及远程访问控制。
This application brief will address many of the power infrastructure challenges that are common in factories, production facilities, and large distribution centers. Provided will be real life, on-site experiences as well as an outline of steps required to overcome these costly challenges. In many cases, the implementation of affordable and easy-to-install modular technology has helped address these issues.
Want to dramatically reduce your CAPEX spend on your next data center buildout? Consider deploying hardwired rack power distribution units (rack PDUs).
Use Raritan’s PX iPDU Series to reliably distribute power for up to sixteen power supplies. The Cisco Nexus 7718 is an 18-slot chassis with 18 front-accessible vertical module slots and front-to-back airflow and an integrated cable management system.
Use Raritan’s PX iPDU Series to reliably distribute power for up to eight power supplies. The Cisco Nexus 7710 is a 10-slot chassis with 10 front-accessible horizontal module slots and front-to-back airflow and an integrated cable management system.
Use Raritan’s PX iPDU Series to reliably distribute power for up to four power supplies. The Cisco Nexus 7018 is an 18-slot chassis with 18 front-accessible horizontal module slots and side-to-side airflow and an integrated cable management system.
Use Raritan’s PX iPDU Series to reliably distribute power for up to three power supplies. The Cisco Nexus 7010 is a 10-slot chassis with 10 front-accessible vertical module slots and front-to-back airflow and an integrated cable management system.
虽然管理者无法预测灾难何时来袭,他们可以采取步骤以确保届时服务将尽快恢复。 力登的业务连续性和灾难恢复解决方案帮助 IT 人员快速、有效、准确地找出故障、诊断和修复灾后系统故障。
高效的、基于计算机的开发和测试实验室,对于必须不断推出进入市场的创新产品的公司,是必不可少的。 为获得成功,实验室管理者必须克服访问和配置实验室设备和自动化系统的严峻挑战,同时继续减少能源成本。 了解力登如何帮助世界上最具创新精神的公司提高他们的生产率,更快速的回应市场需求。
力登和 Wi-Fi 接入点供应商 Xirrus 创建了一份白皮书,为数据中心呈现复杂的无线监控和管理解决方案。 与物理连接的以太网比较,数据中心基础设施管理(DCIM)使用 Wi-Fi 有许多优点。 以太网需要额外的线缆、交换机、机架空间等。 实际上在许多情况下,完整的 Wi-Fi 解决方案的成本低于以太网仅仅部署线缆的成本。