博客

Common Electrical Terminology

Posted on August 20, 2019 by Gento

Data center managers are on a constant road of innovation. As they implement new solutions, and respond to increasing demands for power, they must consistently consider a wide range of electrical factors. Whether you are exploring the benefits of high-power rack PDUs with sensors, or just beginning to delve into best practice approaches to reduce the carbon footprint of data centers, the following electrical term definitions can help you to better understand the intricacies of rack PDUs. 

Common Electrical Terminology Involved With Rack PDUs

Active power (Watt): The active power refers to the watts that are being drawn by an IT device. It is important to note that 1 watt of electricity equals 1 watt of heat within IT equipment. Understanding the heat load of IT equipment is vital to proper load balancing. 

Apparent power (VA): The product of the voltage applied to the IT device times the current drawn by the equipment. The VA is always equal to or larger than the active power. It is calculated by combining the reactive power and true power. The assigned VA rating is used for sizing wiring and circuit breakers.

Current (Amp): The rate of flow of electrons, ions, or holes in a conductor or medium between two points. The difference in potential is measured in amperes (amps), which are the ratio of the voltage to the resistance.

Ground: The ground is a conducting body that is attached from the object and connected (i.e. grounded) to the earth. It is used to safely direct stray currents into the ground.

Line: The line is an electrical conductor. For example, a single-phase system will typically have one line, while a three-phase system has three lines.

Neutral: The neutral is the electrical conductor that creates a return path for the voltage supplied by a line. However, it is important to note that the neutral itself is not a source of voltage.

Voltage (Volt): A volt is an electromotive force. It refers to the difference in electrical potential, by measuring the current times X the resistance.

4-wire and 5-wire systems: A 4-wire rack PDU consists of one ground wire and three lines. A 5-wire system is the same as the 4-wire system but with the addition of a neutral wire.

Three-phase Delta “∆“: This configuration gets the name Delta because a schematic drawing of it has three transformers forming a triangle or the Greek letter Delta. The three lines connect to the three “corners” of the triangle.

Three-phase Wye “Y“: This configuration gets the name Wye because a schematic drawing of it has three transformers meeting in the center forming the letter “Y”. The three lines connect to the three “branches” of the “Y” and the neutral connects to the center.

Discover The True Power Of The Right Electrical Configurations

In conclusion, one thing is certain, the right electrical configurations are vital to the success of your data center.  Discover the best in class solutions to power management, load distribution, security, and data center management with the help of the Raritan team. Contact Raritan to learn more. 
 

Other Blog Posts

数据中心趋势:机柜密度和停机率呈上升态势
Posted on March 18, 2021
The Impact of COVID on the Mission Critical Industry
Posted on March 12, 2021
Riding Out the Pandemic: The Importance of SmartSensors for Remote Management
Posted on March 8, 2021
Will Governments Force the Data Center Industry to Become More Energy Efficient with Green Data Center Laws?
Posted on March 2, 2021
KVM交换机和BIOS级访问
Posted on February 24, 2021

View all Blog Posts

力登官方微信公众号

力登官方微信公众号
cn-blogfollow

近期活动

Data Cloud India
February 5-6, 2020  •  Mumbai, India
Industrial Automation
April 24, 2020  •  Tainan, Taiwan
DigiTimes Data Center Forum Taipei
May 8, 2020  •  Taipei, Taiwan
Cloud & Data Center Convention (Wmedia)
May 14, 2020  •  Manila, Philippines
Industrial Automation
May 14, 2020  •  Taipei, Taiwan

View all Events

力登最新新闻

力登公司推出MasterConsole®数字双显示器KVM切换器
Posted on February 18, 2021
Legrand Data, Power and Control Division Announced as Finalist in Six Categories at DCS Awards 2020
Posted on November 9, 2020
力登公司(Raritan)推出新型智慧型机架控制器(SRC),用于智能地管理数据中心和关键基础设施中的环境和安全信息
Posted on November 9, 2020
Legrand India Launches Datacenter Infrastructure Solution for the addressable market size of INR 3000 crores
Posted on August 23, 2020
力登公司推出面向中小型企业的全新一代KVM-Over-IP交换机和串行访问
Posted on March 16, 2020

View all news