博客

How Can Data Centers Save Realty Costs by Increasing Rack Density?

Posted on October 21, 2015 by Gento

Imagine a data center in New York or Shanghai or Bangalore for that matter, looking at expansion. With leases and rentals hitting the roof, what is the most economical way for them to expand? A horizontal growth will only incur additional expenses of cabling, cooling and not to mention gigantic real estate. Adding to the operating cost can only put pressure on bottom-line. Data centers have a continuous need to look at ways to be cost effective in order to get a competitive edge in the crowded market space. With the realty rates reaching the sky, data centers are challenged to maximize benefits from existing space without impacting their expansion plans. If this sounds like a complex problem, the solution is simple – find ways that provide more computing power for less cost per square foot. Now, the question is how do we put this simple solution to work? The answer lies in vertical expansion powered by the right choice of power distribution units.

Vertical Expansion – a New Mantra for Data Center Efficiency

Vertically scaling up the data center will allow rapid expansion of power density by extending power distribution all the way to the individual rack and cabinets, without undertaking any major structural changes in the data center. Data center designers and managers are beginning to understand the importance of efficiency in building up and replacing the sprawl with higher density racks.

Most data centers with the legacy infrastructure cater to 4-5 KW per rack while the requirement has shot multiple times – beyond 20 KW per rack in many cases. With the high volume big data streams becoming a norm, data centers need to be prepared to handle more density per rack and therefore must look at maximizing their capabilities. Keeping this in mind, data centers are already moving toward high-density computing environments with new and dense servers being deployed. The primary reasons cited for moving to higher densities include saving facility space and reducing energy costs.

 

Right PDUs in Addition to High Density Racks Go Hand in Hand

With changing market demands, data centers need to plan ahead and be ready for future challenges. Though high density racks are playing a pivotal role in increasing ROI of various organizations, power distribution units are equally important. It helps to be prepared and invest in PDUs that are designed with the future requirements in mind. The data centers of the future must have a longer lifecycle and as such need a lot of careful strategizing. One important part of the expansion plan is the choice of PDUs. Balance tilts in favor of PDUs that are capable of extending power distribution all the way to the individual rack and cabinets, without undertaking any major structural changes. Increasing power density by packing more resources per rack is an obvious choice, but then, care is to be taken to ensure this does not escalate operating cost by putting pressure on cooling efficiency or increase cabling cost manifold.

Three-Phase Rack PDUs – the Ideal Approach Towards Vertical Spacing

Three-phase systems enable the consolidation of power circuits with three-phase PDUs that have a much greater distribution capacity. Intelligent solutions like three-phase PDUs which run a single three-phase power cable to rack, reducing bulk cabling at bottom. This approach not only frees the space but also increases airflow, bringing down the cost of cooling. Higher voltages at lower currents means smaller cables, which use less copper, weigh less, take up less space and cost less. By eliminating voltage transformations, 400V power reduces energy cost up to approx. 2% - 3% relative to 208V and approx. 4% - 5% relative to 120V.

Smart is in and data centers must have smart ways to monitor, report and operate. PDUs must also provide visibility to improve operational efficiency. Proper power usage monitoring, voltage levels, humidity and other environmental factors is essential. It is also crucial to maintain pressure and airflow at inlet and outlet level for the health of the data centres. Having a separate monitoring system for each device is cumbersome and impractical, not to mention cost intensive. PDUs that combine power distribution capabilities with smart monitoring and visualization are the best bet.

Customizability is an important aspect for any infrastructure that data centers invest in. PDUs that come with a strict integration framework become an impediment to easy adoptability. Most data centers look for PDUs that are not only compact but are customizable to their requirements including number of outlets, phase balancing, staggered outlets, cord lengths, multiple inputs, remote power control, individual outlet metering, high-power for blade servers and high-density applications, or even 400V power distribution. Three phase PDUs with a capacity to serve 65KW per rack have also made an appearance in the market, providing data centers an unmatched opportunity to scale for huge data flow.

Conclusion

To sum up, undoubtedly data centers must reinvent themselves in view of the rising challenges. The demands are increasing and so is competition. Staying ahead of the herd requires a whole new perspective that looks at every inch of the available space with a critical eye and build processes that not only sustain the operations today but are capable of scaling in the future. Utilizing each rack optimally and vertically expanding seems to be the path towards viable and sustained growth. Data centers that can increase rack density will definitely have higher cost efficiencies in this highly competitive market.

 

To learn more about high power density deployments, watch our webinar,"Overcoming the Challenges of High Power Density Deployments".

Other Blog Posts

数据中心趋势:机柜密度和停机率呈上升态势
Posted on March 18, 2021
The Impact of COVID on the Mission Critical Industry
Posted on March 12, 2021
Riding Out the Pandemic: The Importance of SmartSensors for Remote Management
Posted on March 8, 2021
Will Governments Force the Data Center Industry to Become More Energy Efficient with Green Data Center Laws?
Posted on March 2, 2021
KVM交换机和BIOS级访问
Posted on February 24, 2021

View all Blog Posts

力登官方微信公众号

力登官方微信公众号
cn-blogfollow

近期活动

Data Cloud India
February 5-6, 2020  •  Mumbai, India
Industrial Automation
April 24, 2020  •  Tainan, Taiwan
DigiTimes Data Center Forum Taipei
May 8, 2020  •  Taipei, Taiwan
Cloud & Data Center Convention (Wmedia)
May 14, 2020  •  Manila, Philippines
Industrial Automation
May 14, 2020  •  Taipei, Taiwan

View all Events

力登最新新闻

力登公司推出MasterConsole®数字双显示器KVM切换器
Posted on February 18, 2021
Legrand Data, Power and Control Division Announced as Finalist in Six Categories at DCS Awards 2020
Posted on November 9, 2020
力登公司(Raritan)推出新型智慧型机架控制器(SRC),用于智能地管理数据中心和关键基础设施中的环境和安全信息
Posted on November 9, 2020
Legrand India Launches Datacenter Infrastructure Solution for the addressable market size of INR 3000 crores
Posted on August 23, 2020
力登公司推出面向中小型企业的全新一代KVM-Over-IP交换机和串行访问
Posted on March 16, 2020

View all news