关于我们

Raritan Announces New SmartSensors™ for Accurate Insights on Data Center Environmental Health

—SmartSensors Win Industry Award —

Posted on January 30, 2019

SOMERSET, NJ (January 22, 2019)Raritan® — a brand of Legrand, and a leading provider of intelligent data center management and rack power distribution solutions — today introduced new monitoring sensors to provide data center operators an accurate picture of environments at the rack, aisle, and facility level, and of potential risks. Raritan’s new SmartSensors™ can monitor a cabinet’s temperature, humidity, airflow, and air pressure — as well as detect water leaks, vibrations, and unauthorized openings of cabinet doors.

With compute loads and deployments of double-digit kW cabinets on the rise, accurate monitoring of environmental dynamics is necessary to provide safe conditions for servers to operate. Raritan’s next-generation environmental sensors provide the industry’s highest metering accuracy at +/- 0.5 °C for temperature sensors and +/- 2.5% for relative humidity sensors.

“By using Raritan’s SmartSensors, data center managers can accurately monitor the exact input and output temperature, humidity, and airflow for every single cabinet in order to fine-tune cooling and humidity requirements and to optimize efficiency,” says Paul Mott, Global Technical Product Manager at Raritan.  “Generating data at the cabinet level allows for better analysis and opportunity to optimize operations and reduce energy costs.” 

SmartSensors come in different configurations — such as a combined temperature and humidity sensor — to make it easy to measure the cold and hot aisles, and position the sensors top, middle, and bottom in the cabinet — as recommended by ASHRAE. Raritan also offers SmartSensors that detect water leaks and vibrations.  For security, contact closure sensors are available to monitor cabinet door openings/closings.
“Like the proverbial miner’s canary, Raritan’s SmartSensors provide early warning alerts to potential problems, such as hot spots, that could jeopardize the performance and life of IT assets,” adds Mott. 
The collected sensor data helps to reveal trends over time. For additional insight, information gathered by sensors can be monitored and analyzed by DCIM (Data Center Infrastructure Management) software for tracking trends and generating reports. Users, for example, can on a dashboard compare the data from sensors to the environmental envelope of a psychrometric chart to ensure that adequate cooling is where it needs to be.

SmartSensor Benefits

  • Save on cooling by confidently raising data center temperatures.
  • Check airflow and air pressure to and from racks to prevent hot spots and bypass recirculation.
  • Make strategic decisions on cooling design and containment.
  • Set thresholds and alerts to monitor on-site and remote facilities.
  • Improve data center uptime by receiving alerts for any fault conditions.

Availability
Raritan SmartSensors are available worldwide. 

Without disrupting operations, Raritan’s plug-and-play SmartSensors can be installed into Raritan’s PX® intelligent PDUs thereby cost effectively leveraging the existing network layer in racks provided by the PDUs. The sensors also can be deployed as plug-and-play options for Raritan’s EMX rack controllers, PX inline meters, rack transfer switches, and branch circuit monitors. Removable sensor heads are available to help maintain the accuracy of the temperature/humidity sensors.

Visit here to learn more about Raritan’s SmartSensor — which was awarded a 2018 IoT Product of the Year Award by IoT Evolution Magazine.

About Raritan
Raritan, a brand of Legrand, is a global leader in intelligent rack PDUs, KVM switches, and other data center infrastructure monitoring and management solutions. Raritan’s innovations improve the reliability, efficiency, and intelligence of data centers and server rooms around the globe — including those of the top Fortune 500 companies, such as Cisco, Dell, Google, HP, IBM, Intel, and Microsoft. To learn more, visit Raritan.com, LinkedIn or Twitter.

About Legrand and Legrand, North and Central America
Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines that includes AFCO Systems, C2G, Cablofil, Chief, Da-Lite, Electrorack, Finelite, Luxul, Middle Atlantic Products, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Sanus, Solarfective, Vaddio, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819) www.legrand.us.

# # #

All product and company names herein may be trademarks of their registered owners.

View by Category
Monthly Archives
More Recent News
力登公司推出MasterConsole®数字双显示器KVM切换器

— 新的交换机可让用户高效地使用带有无边界鼠标的双显示器 —

Posted on February 18, 2021
Legrand Data, Power and Control Division Announced as Finalist in Six Categories at DCS Awards 2020
Posted on November 9, 2020
力登公司(Raritan)推出新型智慧型机架控制器(SRC),用于智能地管理数据中心和关键基础设施中的环境和安全信息

— 智慧型传感器(SmartSensors)将温度、气流、水/泄漏和触点闭合的状态数据传输到新型智慧型机架控制器(SRC),为实时决策和管理数据中心提供关键的数据支持 —

Posted on November 9, 2020
Legrand India Launches Datacenter Infrastructure Solution for the addressable market size of INR 3000 crores
Posted on August 23, 2020
力登公司推出面向中小型企业的全新一代KVM-Over-IP交换机和串行访问
Posted on March 16, 2020