主页 » 博客
Posted on October 30, 2017 by Gento
Modern data center managers are constantly being asked to do more with less, and a data-driven approach can mean the difference between success and failure. But how do you identify which Key Performance Indicators (KPIs) are right for your organization?
Join Sunbird for our next live DCIM webinar, Data Center KPIs to Optimize Capacity Utilization, to explore how making the most of your data can help you maximize the value of your data center resources.
In this webinar, you’ll learn:
Time: 2PM ET
Date: Tuesday, November 7, 2017
Register now to secure your spot!
Posted on October 30, 2017 by Gento
随着市场上数据中心需求的猛增, 不论是大企业还是小公司,托管这一概念俨然已成为各类企业更受欢迎的选择。主机托管(”Colo”)设施运行并将共享数据中心空间出租给各个租户客户,而非单独自行管理自己数据中心的公司。
刚刚创立的公司或是一些想要扩大数据中心的大型机构,应该会从托管这一选择中获益。为帮助您更好地了解托管的含义,我们列举了以下有关托管的优势和挑战,让您的数据中心“结伴飞翔”而不是“单飞”。
Posted on October 30, 2017 by Gento
Data center growth is on the rise, spurred by the digital age that we're now living in. A major component and driver of this expansive growth is the popularity of the ‘Internet of Things’. Data center construction is expected grow at an incredible rate of 21% per year between now and 2018. They're such an essential part of our daily lives that 23 states now offer tax incentives to help attract new projects, while 16 others states offer tax incentives that total a combined $1.5 billion.
Posted on October 30, 2017 by Gento
Many people don't realize that the most significant cause of data center downtime, to the tune of an incredible 70% by most estimates, actually has to do with your employees, more specifically, human error. It's a very serious problem that will only get worse if not corrected upfront, but luckily there are a few key steps that you can start taking today to help mitigate risk from these types of issues moving forward.
Posted on October 30, 2017 by Gento
Would you like to put a hard power capacity limit on a rack to ensure failover success or put a limit on a set of racks?
Load shedding can be the answer to preventing rack circuit-failover failure.
When dealing with PDUs there are already limits to the load capacity of a single device. It comes in the form of floor PDU circuit breakers. However, the capacity limit of a rack can exceed the limit of a single rack circuit. This is due to the fact that you typically load balance between two or more circuits. In other words, each circuit could be under capacity but when you add the loads together (loss of one circuit/failover) you exceed the capacity of one of those circuits. Under these circumstances, you could lose the whole rack because a failover would not succeed.