The Raritan Blog

KVM Switches & BIOS-Level Access - Why is it so Important?

Jessica Ciesla
December 1, 2020

It is often said that KVM switches provide “BIOS-Level  Access” and this is a big advantage of KVM Switches over other forms of remote management.  But what does this actually mean and why is it so important?  How do KVM Switches provide this and why is it important?  This blog introduces these topics.  A future blog will cover more advanced features and topics.


COVID, KVM, and WFH

Jessica Ciesla
October 26, 2020

In a report released last month by 451 Research, the overall prognosis for IT spending during the pandemic is not a good one. The report notes that their leading indicator plunged “. . . to the worst level over the last decade.” Given the impact of the pandemic on the global economy, and on small businesses in particular, it is no surprise that these overall gauges of spending in our industry are showing negative numbers. One of the few bright spots in the report, however, is the fact that the pandemic “. . . compels organizations to adopt work-from-home business practices,” a category that has seen a 41% growth amidst a sea of negative numbers. 


LX II Combination LCD Drawer and KVM-over-IP Switch

Jessica Ciesla
October 6, 2020

Economical Remote Management and At-the-Rack Access in a Single Product!

Do you need web-based, remote management of computer and networking equipment?   Do you also need at-the-rack access of computer equipment?    And would you like an economical, easy-to-use product that can do both?

If so, Raritan’s Dominion LX II – LED combination LX II KVM Switch and T1700-LED LCD drawer models can do all of that and more!


Blazing Virtual Media Speed for the Dominion KX IV - 101

Jessica Ciesla
August 12, 2020

When we talk about the Dominion KX IV -101 as Raritan’s fastest KVM-over-IP switch, we are usually focused on its ability to support 4K video or 1080p video at 60 frames per second. But video isn’t the only area where the KX IV-101 shines!  Due to its all-digital architecture and its direct USB connection to the target computer, the KX IV-101 supports virtual media much faster than our current generation Dominion KX III switches.  


The New Dominion LX II: Why You Should Trade Up

Jessica Ciesla
April 2, 2020

Looking for an economical KVM solution? This blog discusses features included in the new Dominion LX II, and why it would be beneficial for you to trade up from the original Dominion LX. 

The new Dominion LX II from Raritan is the latest in a line of products designed with the small to midsize business IP KVM switch user in mind.  Our new unit is designed to provide economical, Java-free, BIOS-level remote access to between 8 and 16 servers as well as virtual media.  The new Dominion also supports connections up to 15 frames-per-second at a resolution up to 1080p and 1200p.  With six different options available, the next generation LX II is poised to become the leading SMB IP KVM switch on the market today.


Page 3 of 38 pages  < 1 2 3 4 5 >  Last ›