Home » Raritan Blog
Dorothy Ochs
July 13, 2012
Khaled Nassoura, Raritan’s General Manager of DCIM Solutions, will present at 2:30 in Hall 2. The presentation title is “DCIM: Intelligent Infrastructure Management to Improve Data Center Efficiency and Utilization.” The abstract and other details can be found online. And don’t forget to stop by our booth #7 to see our latest solutions and meet the local team.
We have a limited number of complimentary passes for end users. If you would like one, please marketing@raritan.com.
http://www.datacenterdynamics.com/conferences/2012/san-francisco-2012
June 27, 2012
In previous blog entries, we’ve seen that a truly 100% homogeneous data center environment is far from the norm. Rare is the data center that relies on a single server vendor or server type. As a result, multiple management tools are often used, which can be a nightmare in its own right. Managing a bunch of management tools seems a little redundant.
But maybe you are a one-stop-shop. Perhaps you’ve configured all your Dell blade servers for easy management access via DRAC. You’re on easy street, right? Or you’ve virtualized. You’re the resident VMware hero and you’re saving more money on hardware and power than you originally thought possible. But you have all those DRAC connections on a secondary LAN. What if you lose access? Or you find yourself unable to restart a virtual machine through vCenter? What then?
James Cerwinski
June 22, 2012
Many dcTrack customers have expressed a desire to elevate dcTrack’s position within their operations by integrating dcTrack with their Remedy CMDB and change ticket system.
dcTrack has the open API for such an integration and is a member of the BMC Software Technology Alliance Program.
Pinebreeze Technologies Inc. has integrated BMC Remedy with dcTrack
“The BMC Remedy connector enables Remedy change tickets to electronically flow into dcTrack to reduce human error and ensure all changes are captured in dcTrack”
Your options are not limited to BMC.
June 11, 2012
San Diego Convention Center, San Diego, CA
June 11-14, 2012
Booth # 437, Pod # E3
Today Raritan announced that its PX intelligent power distribution units (iPDUs) are Cisco® EnergyWise™ certified. A wide array of useful energy information is collected from servers and devices connected to Raritan’s networked iPDUs, and shared with Cisco EnergyWise, so that organizations can gain a better understanding of their power footprint and energy costs.
Come to see our presentation on “Cisco EnergyWise and Raritan’s Dominion PX: What does it mean for energy efficiency & What does it mean for extension into the desktop space”. Presentations will held daily at the UABU EW & UPOE Pavilion.
May 11, 2012
Join Raritan at the Uptime Institute Symposium (http://symposium.uptimeinstitute.com/) in the Santa Clara Convention Center, May 14-15, 2012. Raritan will be discussing some of the anomalies and issues when metering current in three-phase power deployments. We will also present approaches to monitoring power consumption and practical, tactical methods to increase efficiencies.
Presentation - Tuesday, May 15, 2012, 2:40-3:10pm, Ballroom F
Raritan Booth# 221
*Source: http://symposium.uptimeinstitute.com/schedule/1664-adp-data-center-optimizing-three-phase-power-distribution-for-higher-densities